How could I run PWM on MKW01Z128 pin PTC1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How could I run PWM on MKW01Z128 pin PTC1

3,273 Views
sergiiparadiuk
Contributor II

I found info about FTM_DRV_Pwm, but it couldn't find all structures for my platform. I enabled #define FSL_FEATURE_SOC_FTM_COUNT (1) and got a lot of errors:

Error[Pe020]: identifier "FTM_Type" is undefined 

....

What is wrong?

Tags (1)
0 Kudos
Reply
11 Replies

3,109 Views
sergiiparadiuk
Contributor II

Hello,

I found other libs for this and started to use it, but can't still run PWM on the pin PTC1 (in the doc it uses TPM module 0 Channel 0). I use the next code:

tpm_general_config_t tpmCfg =
{
    .isDBGMode = true,//0,
    .isGlobalTimeBase = 0,
    .isTriggerMode = 0,
    .isStopCountOnOveflow = 0,
    .isCountReloadOnTrig = true,//0,
    .triggerSource = kTpmTrigSel8//kTpmTrigSel0,
};
tpm_pwm_param_t param =
{
    .mode = kTpmEdgeAlignedPWM,
    .edgeMode = kTpmHighTrue,
    .uFrequencyHZ = 100000U,
    .uDutyCyclePercent = 50U,
};
tpm_status_t status;

PORT_HAL_SetMuxMode(PORTC,1u,kPortMuxAlt2);
TPM_DRV_SetClock(TPM0_IDX, kTpmClockSourceExternalClk, kTpmDividedBy2 );
status = TPM_DRV_Init(TPM0_IDX, &tpmCfg);
status = TPM_DRV_PwmStart(TPM0_IDX, &param, 0);
...

What is wrong? I don't see any output on PTC1, all time 0 Volts.

0 Kudos
Reply

3,109 Views
mjbcswitzerland
Specialist V


Hi Sergii

TPM0_CH0 is ALT 4 on PTC1 and not ALT 2.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html

Free Open Source solution: https://github.com/uTasker/uTasker-Kinetis
Working project in 15 minutes video: https://youtu.be/K8ScSgpgQ6M

For better, faster, cheaper product developments consider the uTasker developer's version, professional Kinetis support, one-on-one training and complete fast-track project solutions to set you apart from the herd : http://www.utasker.com/support.html

0 Kudos
Reply

3,109 Views
sergiiparadiuk
Contributor II

Hello,

Thanks,it was helped. Now works.

0 Kudos
Reply

3,109 Views
sergiiparadiuk
Contributor II

I have other issue. I setuped PWM on frequency 50 Hz. 

I can control duty cycle from 0 to 100% with precision 1. For example 0,1,2,3,4 ..100.

Can I control t wit better precision? For example 0,2%.

0 Kudos
Reply

3,109 Views
mjbcswitzerland
Specialist V

Sergii

The PWM precision depends on the counter match value used to generate your base frequency. Since you have a low frequency the counter match will be a high value (optimally it should be set - using an appropriate clock pre-scaler - to be a large value as close to 0xffff as possible. This will allow high precision (in the best case approaching 0.002%).

Therefore, check the counter match value presently used, optimise it if possible, and then make use of the fine control (in case the API that you are presently using is restricting it).

Regards

Mark


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

0 Kudos
Reply

3,109 Views
sergiiparadiuk
Contributor II

Thanks for the response. Could you give some example how to do it?

пт, 13 апр. 2018 г., 3:02 mjbcswitzerland <admin@community.nxp.com>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: How could I run PWM on MKW01Z128 pin PTC1

reply from Mark Butcher

<https://community.nxp.com/people/mjbcswitzerland?et=watches.email.thread>

in Kinetis Microcontrollers - View the full discussion

<https://community.nxp.com/message/1005043?commentID=1005043&et=watches.email.thread#comment-1005043>

0 Kudos
Reply

3,109 Views
mjbcswitzerland
Specialist V

Hi

See what value is being written to the FTMx_MOD register (this is your time base).
Then you can control your output channel's FTM_CV register with value from 0...FTMx_MOD value and its resolution is given by (1/FTMx_MOD * 100)%

Regards

Mark


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

0 Kudos
Reply

3,109 Views
sergiiparadiuk
Contributor II

Thank you for the response.

Is it possible to do it from API?

I use TPM_DRV_* API to set up PWM...

0 Kudos
Reply

3,109 Views
sergiiparadiuk
Contributor II

And one more things.

How is possible to run watch dog for MKW01Z128? I tried lib #include "fsl_wdog_driver.h", but It can't find WDOG_Type structure, it looks like this structure is not exist for this mcu.

 

0 Kudos
Reply

3,109 Views
sergiiparadiuk
Contributor II

and how can I use sleep mode? (couldn't find API)

0 Kudos
Reply

3,109 Views
mjbcswitzerland
Specialist V

Sergii

I am sorry but I don't use the APIs so can't help more.

Regards


Mark


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html

0 Kudos
Reply