How can J-Flash flashing MKE06Z128VLK4?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can J-Flash flashing MKE06Z128VLK4?

1,102 次查看
matherinewang
Contributor III

Hi Friends,

I prepare use SEGGER J-Flash for MKE06Z128VLK4.

But when i execute File->Open Project, i find there are many *.jflash files here but seems no one for MKE06Z128VLK4.

how can i flash MKE06Z128VLK4 with J-Flash? is it means i can't do it? Thanks in advance

标签 (1)
0 项奖励
回复
1 回复

733 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi matherine wang,

You can use “Create a new project” instead of "Create project from template".

Just refer to the following step:

1: Create a new project

53.jpg

2: do Project settings

54.jpg

3: Select KE06Z128VLK4, Then save the .jflash, this is what you needed.

pastedImage_0.png

Wish it helps your.

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复