Hi There, I wanted to know if I could use the CMSIS header files from the kinectis SDK or sample code to add KINECTIS support to other projects such as RIOT, CHIBIOS, opencm3?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi There, I wanted to know if I could use the CMSIS header files from the kinectis SDK or sample code to add KINECTIS support to other projects such as RIOT, CHIBIOS, opencm3?

838件の閲覧回数
raghavaaditya
Contributor I

-

ラベル(1)
0 件の賞賛
返信
1 返信

772件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Raghava,

Although I do not know the CHIBIOS OS and the RIOT game, I think it is okay to use CMSIS header from the Kinetis SDK, because we provide the source code of CMSIS and header file, you can add the source code file to your system.

Hope it can help you.

BR

XiangJun Rong

0 件の賞賛
返信