Hi, I am working with kinetis W 21D256 micro-controller. My application is battery powered so that I want to optimize power as much as possible... All I need to do is switch between Run Mode and Vlpr mode via RUN.I'm changing the mcg mode to BLPI and turning OFF the clock monitor,SMC_PMPROT[AVLP]) is set,SIM_CLKDIV1_OUTDIV1=0,SIM_CLKDIV1_OUTDIV2=1,SIM_CLKDIV1_OUTDIV4=4. But PMC REGONS bit is not turning 0. Is there anything else that I need to do. Please give me any suggestions. Best Regards, Madan
Hello Madan,
You need to accomplish a specific routine in order to change to VLPS mode (low power mode) from RUN mode. There is an example (lwirelessUART from SMAC folder) included in Beekit Wireless Connectivity Toolkit (BeeKit Wireless Connectivity Toolkit|Freescale) that shows you how to switch to VLPS in run time. (Function called WUApp_PrepareToEnterLowPower accomplishes this routine, it is located at main.c file) Hope this can help you as guidance.
Best Regards,
Isaac Avila
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Madan,
Have you changed to VLPR mode successfully?
Regards,
Isaac
Hi Madan M,
Sorry for giving you reference about VLPS instead of VLPR mode.
You can check this application note about Power Magaement for Kinetis (http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf)
In this AN, you can notice in section 2.5.3 (in document it is written as 2.5.2 but it was a typo error) the sequence to enter in VLPR:
Remember to set PMPROT[AVLP] = 1 to allow MCU to enter to VLPR mode.
You can check this AN for more information.
If you problem persists please let me know it.
Best Regards,
Isaac
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------