Hey Guys, is it possible to use the MKL25Z FRDM Board to program the MKL15Z128CAD4R?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hey Guys, is it possible to use the MKL25Z FRDM Board to program the MKL15Z128CAD4R?

91,814 次查看
nikotheodoridis
Contributor I

I've seen something about the USBDM but could not find the compatibility from a 2X series to a 1X series.

As well I am using KDS and not the code warrior.

best regards

0 项奖励
回复
3 回复数

1,106 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Niko,

Do you meaning download the code about MKL15Z128CAD4R in to the board FRMK-KL25,

yes ,it can .

pastedImage_0.png

And when you debug, please configure the debug view to KL25z128 chip .

Hope it helps

Alice

0 项奖励
回复

1,106 次查看
nikotheodoridis
Contributor I

Oh, I think you got me at the wrong and of the stick.

As far as I know you can use the FRDM MKL25Z Board as a debugger for external devices.

On our own board we are using the MKL15Z128CAD4R.

Therefore I want to know if it is possible to use the external debug function from the FRDM Board to debug our MKL15ZCAD4R?

Best regards

Niko

Von: Alice_Yang

Gesendet: Freitag, 29. April 2016 10:35

An: Nikolaos Theodoridis

Betreff: Re: - Hey Guys, is it possible to use the MKL25Z FRDM Board to program the MKL15Z128CAD4R?

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Hey Guys, is it possible to use the MKL25Z FRDM Board to program the MKL15Z128CAD4R?

reply from Alice_Yang<https://community.freescale.com/people/Alice_Yang?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion<https://community.freescale.com/message/640279?et=watches.email.thread#comment-640279>

0 项奖励
回复

1,106 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Niko,

Sorry to reply to so late, have your problem be resolved ?

If not ,there is a tutorial about use the FRDM-KL43 board to debug external board,

https://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/  

it is the same debug chip on FRDM-KL25 and FRDM-KL43, so the method is the same,

hope it can help you .

BR

Alice

0 项奖励
回复