Help with KwikStik j-link flashing external device.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Help with KwikStik j-link flashing external device.

跳至解决方案
1,924 次查看
luisf_rossi
Contributor II

Hi, i am trying to use the KwikStik j-link to flash an external Kinetis. For some reason it is not working and CodeWarrior is retrieving a message saying it could not reset the Kinetis.

 

I even tryed to remove the kinetis on the KwikStik board but with no change.

 

The Kinetis connections can be seen on the atachement. Thats just a piece of the board but related to kinetis there are just some extra decoupling network on other sheets.

 

The cable and pinheaders i am using are the sugested by the manual.

the j-link connector is pretty close to the kinetis..

 

 

Any help is appreciated.

0 项奖励
回复
1 解答
1,389 次查看
luisf_rossi
Contributor II

Ok got the problem.. athought the kwikstick is the Version 4 it still can't program external devices with the switch off.. turning on worked here...

 

Thank you

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,390 次查看
luisf_rossi
Contributor II

Ok got the problem.. athought the kwikstick is the Version 4 it still can't program external devices with the switch off.. turning on worked here...

 

Thank you

0 项奖励
回复