Help configuring MK40X256VMD100 on the tower board. Is it to old?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help configuring MK40X256VMD100 on the tower board. Is it to old?

1,095件の閲覧回数
markosiponen
Contributor III

I want to use a tower board (Kinetis K40). It has a MK40X256VMD100.


I want to configure the clocks and flexCAN using the processor expert. But I can't find the MCU in the list when creating a new project.


I read than MK40X256VMD100 was replaced with MK40DZ10.

What MCU should I select in processor expert?

0 件の賞賛
返信
1 返信

965件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello:

If you use TWR-K40X256, then when creating the project you can go with MK40DX256Z or PK40X256 (under 100 MHz).

K40_Rev1.png

Also from the CPU component in Processor Expert, make sure to select the MAPBGA option:

MAPBGA_Package.png

Hope this helps!


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信