Help, I'm new and I can't find the FRDM-KL25Z Drive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help, I'm new and I can't find the FRDM-KL25Z Drive

Jump to solution
1,050 Views
davehaas
Contributor I

I am new to this - followed start-up directions (I thought) and did see the drive once or twice - but can't get it back -THE LED prgrm is running, the slider sensor adjusts intensity - when I boot in Bootloader mode the Bootloader drive comes right up.  I can't find any troubleshooting help or instructions other than the community.

I',m through the quick start-up instructions to where I'm supposed to copy example programs to that drive - but it's lost

Can anyone please help me?  THanks,

Dave Haas

0 Kudos
Reply
1 Solution
939 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
1 Reply
940 Views
BlackNight
NXP Employee
NXP Employee

Hi,

this article gives an overview and tips:

OpenSDA on the Freedom KL25Z Board | MCU on Eclipse

and if you are going to debug your board, then this article might help:

The Freescale OpenSDA Trap: “No Device Available”, or something like that…. | MCU on Eclipse

0 Kudos
Reply