Help, I'm new and I can't find the FRDM-KL25Z Drive

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help, I'm new and I can't find the FRDM-KL25Z Drive

ソリューションへジャンプ
1,035件の閲覧回数
davehaas
Contributor I

I am new to this - followed start-up directions (I thought) and did see the drive once or twice - but can't get it back -THE LED prgrm is running, the slider sensor adjusts intensity - when I boot in Bootloader mode the Bootloader drive comes right up.  I can't find any troubleshooting help or instructions other than the community.

I',m through the quick start-up instructions to where I'm supposed to copy example programs to that drive - but it's lost

Can anyone please help me?  THanks,

Dave Haas

ラベル(2)
0 件の賞賛
返信
1 解決策
924件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
1 返信
925件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi,

this article gives an overview and tips:

OpenSDA on the Freedom KL25Z Board | MCU on Eclipse

and if you are going to debug your board, then this article might help:

The Freescale OpenSDA Trap: “No Device Available”, or something like that…. | MCU on Eclipse

0 件の賞賛
返信