Hello community. just received a kwikstik-40 and am unable to charge the battery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello community. just received a kwikstik-40 and am unable to charge the battery

908 Views
jeffpurcell
Contributor I

Hello community.  just received a kwikstik-40 and am unable to charge the battery via USB. It powers up and runs while connected to USB but even after 5 hours it only shows 1 bar of charge and not enough to power up on the battery.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

828 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Jeff

As you can find, there is a ON/OFF switch on another side of Kwikstik_K40. Did you turn it on when you want to use this board?

If yes, there is still no 3.3V power. I think you need to check if battery still has energy.

Hope my reply can help you. Thanks.

Best Regards

Paul

0 Kudos
Reply