Hi
I want to use arm_cfft_radix4_init_q15() and arm_cfft_radix4_q15() function from CMSIS 3.2 library . I am unable to find any good resources or any examples. I have looked in the documents provided by ARM i.e CMSIS-DSP: Complex FFT Functions but I didn't find it useful. What are the inputs given to these functions I am still not clear with it. I tried writing the codes but it didn't worked
this is how I am calling the functions,
arm_cfft_radix4_init_q15(&arm_cfft_sR_q15_len256, 256, 0, 1); // For init
arm_cfft_radix4_q15(&arm_cfft_sR_q15_len256, az); // For transformation where,
arm_cfft_radix4_instance_q15 arm_cfft_sR_q15_len256 = {256, 0, 1, twiddleCoef_256, armBitRevIndexTable256, 4U, 4U};
and az[512] is an array where the data is stored. Just for testing
float32_t az[512] = {1.2 ,0.0
1.3, 0.0
-------
--------
1.2, 0.0};
my programs hangs and I am not able to print the o/p. I am using Codewrrior 10.5 and want to implement this on FRDM-K20D50M. I posted the query in ARM's community also but I didn't get any response which makes me think if anybody is actually using this library. Please look into the matter.
Kind Regards
Amit Kumar
解決済! 解決策の投稿を見る。
Hi,
I have some good news. Your build of the library has the correct compiler options set, and your applications does as well. However, it appears you are linking the application to the pre-built library provided by CMSIS. This pre-built version does not have -ffunction-sections -fdata-sections set; therefore, the unused data will not be removed.
To link your rebuild of the library correctly into your project you need to make sure you have the following properties set:
and:
Please let me know if this works for you.
Best regards,
Martyn
P.S. For reference the correct compiler settings for library and application are:
Library Compiler:
Application compiler and linker options:
Hi martynhunt
I Tried implementing the CFFT code into my project. It gave an error that m_text overflowed. Then I configured the flex mem and increased the size but still the error was the same and the amount by which it was being overflowed was the same, then I reduced the input buffer size from 2048 to 32 but still the same message. I tested the library by implementing sine, cosine function example code and that is working fine then I tried to implement CFFT example code which still didn't worked. Currently I am using CMSIS 3.2, with codewarrior10.6 and I am implementing this on FRDM-K20D50M board. Attached is my project with built library please have a look into it.
The error snapshot when the data array was 256.
Kind Regards
Amit Kumar
m_text overflowed means that your application is too big, and according to the screenshot it is over by more than 50 KByte.
I have not checked your project, but it looks like your are linking too much?
HI Erich
Thanks for the reply. How do I overcome this error? any suggestions? I checked with reduced array size from 2048 to 32. but the size by which it is overflowing is the same. there is a warning message also which says invalid project path. Is that message of any concern?
Kind Regards
Amit Kumar
Hi,
I have some good news. Your build of the library has the correct compiler options set, and your applications does as well. However, it appears you are linking the application to the pre-built library provided by CMSIS. This pre-built version does not have -ffunction-sections -fdata-sections set; therefore, the unused data will not be removed.
To link your rebuild of the library correctly into your project you need to make sure you have the following properties set:
and:
Please let me know if this works for you.
Best regards,
Martyn
P.S. For reference the correct compiler settings for library and application are:
Library Compiler:
Application compiler and linker options:
Hi Martyn
Thanks for your support. It worked
Kind Regards
Amit Kumar
Hi,
It looks like the GCC linker is pulling in all of the data tables in arm_common_tables.h. See .map file excerpt:
.rodata 0x00005e04 0xc ./Sources/main.o
.rodata 0x00005e10 0x26d58 C:/Users/B45635/Downloads/CMSIS-SP-00300-r3p2-00rel1/CMSIS/Lib/GCC\libarm_cortexM4l_math.a(arm_common_tables.o)
0x00005e10 twiddleCoef_rfft_4096
0x00009e10 twiddleCoef_rfft_2048
0x0000be10 twiddleCoef_rfft_1024
0x0000ce10 twiddleCoef_rfft_512
0x0000d610 twiddleCoef_rfft_256
0x0000da10 twiddleCoef_rfft_128
0x0000dc10 twiddleCoef_rfft_64
0x0000dd10 twiddleCoef_rfft_32
0x0000dd90 armBitRevIndexTable4096
0x0000fd10 armBitRevIndexTable2048
0x00011ad0 armBitRevIndexTable1024
0x000128e0 armBitRevIndexTable512
0x00012c60 armBitRevIndexTable256
0x00012fd0 armBitRevIndexTable128
0x00013170 armBitRevIndexTable64
0x000131e0 armBitRevIndexTable32
0x00013240 armBitRevIndexTable16
0x00013268 armRecipTableQ31
0x00013368 armRecipTableQ15
0x000133e8 twiddleCoefQ15
0x000163e8 twiddleCoefQ31
0x0001c3e8 twiddleCoef_4096
0x000243e8 twiddleCoef_2048
0x000283e8 twiddleCoef_1024
0x0002a3e8 twiddleCoef_512
0x0002b3e8 twiddleCoef_256
0x0002bbe8 twiddleCoef_128
0x0002bfe8 twiddleCoef_64
0x0002c1e8 twiddleCoef_32
0x0002c2e8 twiddleCoef_16
0x0002c368 armBitRevTable
.rodata 0x0002cb68 0x20 C:/Freescale/CW MCU v10.6/MCU/ARM_GCC_Support/ewl/lib/armv7e-m\libc.a(__strtold.o)
This appears to be an issue with how the ARM library behaves when being built with GCC compiler.
Best regards,
Martyn