HOW CAN I IMPLEMENT WIRELESS LIBRARIES ON MY KW41Z PROJECT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HOW CAN I IMPLEMENT WIRELESS LIBRARIES ON MY KW41Z PROJECT

跳至解决方案
982 次查看
jricaurtepino
Contributor II

Hi

I need to use the wireless libraries on my own project. i have already seen the examples and demos. I need the bluetooth libraries. Does anyone know how to do that?

 

Thanks

0 项奖励
回复
1 解答
974 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Not the library, all the file is important. You would better develop the project based on the example.

Or you would better copy all file to your new project. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
975 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Not the library, all the file is important. You would better develop the project based on the example.

Or you would better copy all file to your new project. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------