HOW CAN I IMPLEMENT WIRELESS LIBRARIES ON MY KW41Z PROJECT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HOW CAN I IMPLEMENT WIRELESS LIBRARIES ON MY KW41Z PROJECT

Jump to solution
1,104 Views
jricaurtepino
Contributor II

Hi

I need to use the wireless libraries on my own project. i have already seen the examples and demos. I need the bluetooth libraries. Does anyone know how to do that?

 

Thanks

0 Kudos
Reply
1 Solution
1,096 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Not the library, all the file is important. You would better develop the project based on the example.

Or you would better copy all file to your new project. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
1,097 Views
nxf56274
NXP Employee
NXP Employee

Hi,

Not the library, all the file is important. You would better develop the project based on the example.

Or you would better copy all file to your new project. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------