HAL,IO_TIMEOUT Errors during Layer 3/4 Activation with CLEV663

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HAL,IO_TIMEOUT Errors during Layer 3/4 Activation with CLEV663

2,101件の閲覧回数
dami2048
Contributor I

Hello,

I'm encountering "HAL,IO_TIMEOUT" errors when attempting to activate Layer 3 and Layer 4 on a Desfire EV4 card using the aCLEV663 NFC board (OM26630FDKM).

Setup:

  • Board: CLEV663 NFC board (OM26630FDKM)
  • Card: Desfire EV4 card supplied with the CLEV663 kit
  • Software: NXP NFC Cockpit v8.1.0

Steps Taken:

  1. Successfully loaded the Type A protocol.
  2. Turned on the RF field.
  3. Placed the Desfire EV4 card on the antenna (card is confirmed working).
  4. Attempted Layer 3 activation -> Received "RFProtocolTypeAService:RequestA Failed: HAL,IO_TIMEOUT" and "RFProtocolTypeAService:PerformLayer3Activation Failed: HAL,IO_TIMEOUT" errors.

Additional Information:

  • The card is placed in the antenna RF field.
  • The card is functional..

I would appreciate any assistance in resolving this issue. 

0 件の賞賛
返信
5 返答(返信)

2,050件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @dami2048 

The following steps for your reference.

KellyLi_0-1727259696024.png

 

0 件の賞賛
返信

2,040件の閲覧回数
dami2048
Contributor I

Hello @KaiLi 
Following the steps i get an error on step 3, when i try to activate Layer3

0 件の賞賛
返信

2,007件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @dami2048 

When you try to activate layer 3,  you need to put the card on field, in this case, also get failed, please change another card and try again.

0 件の賞賛
返信

2,063件の閲覧回数
dami2048
Contributor I

sorry its an EV3 card

0 件の賞賛
返信

2,071件の閲覧回数
KaiLi
NXP TechSupport
NXP TechSupport

Hello @dami2048 

Are you sure you are using an EV4 card? It seems that there is no EV4, only EV1/2/3.

0 件の賞賛
返信