Good low-cost debugger for Kinetis K & L-series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Good low-cost debugger for Kinetis K & L-series

跳至解决方案
1,617 次查看
estrack
Contributor II

What's a good choice for a low-cost ($100 to $300) debugger for the Kinetis K series, that should also support the L series?

Needs to work with CodeWarrior 10.2 / 10.3


I suspect OSBDM from EBay is an option, but perhaps slow, as it is used on the tower boards (?), or CYCLONEMAX_PE, but it is $900, or perhaps PnE U-Multilink, but it has caveats as to which versions of CodeWarrior support it?


What do most of you professional devs use for debugging K series micros?

标签 (2)
0 项奖励
回复
1 解答
1,281 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

This is the CW10.3 supported tools:

tools.bmp

J-Link and USB Multilink I think are the cheaper tools.

Best Regards,

Luis

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,282 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

This is the CW10.3 supported tools:

tools.bmp

J-Link and USB Multilink I think are the cheaper tools.

Best Regards,

Luis

0 项奖励
回复