GPIO in L-series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GPIO in L-series

1,587 次查看
Markon
Contributor II

Hi,

I'm preparing project with MKL16Z64VLH4 and I have questions:

1. May I activate interrupt on every port A, B, C, D, E?

2. May I wake up processor with the use of external pin (for instance PTC6) and than use this pin as external interrupt?

标签 (1)
3 回复数

1,399 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Mar Kon

Q1. May I activate interrupt on every port A, B, C, D, E?

A1: No, Kinetis L series does not support all ports interrupt.

Q2. May I wake up processor with the use of external pin (for instance PTC6) and than use this pin as external interrupt?

A2: You can reference chapter "Interrupt channel assignments" in reference manual. There is a table which tell you which port can support GPIO interrupt and which port can only support single interrupt.

Hope my reply can help you.

Best Regards

Paul

1,399 次查看
Markon
Contributor II

Thank you for your answer.

May I ask you about reference manual for MKL16Z64VLH4 because there isn't any connected with this processor on freescale webside?

0 项奖励
回复

1,399 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mar Kon,

    Reference manual for MKL16Z64VLH4 will be recently launched, please pay aattention to the website.

    Best regards!

Jing