GPIO in L-series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

GPIO in L-series

1,637件の閲覧回数
Markon
Contributor II

Hi,

I'm preparing project with MKL16Z64VLH4 and I have questions:

1. May I activate interrupt on every port A, B, C, D, E?

2. May I wake up processor with the use of external pin (for instance PTC6) and than use this pin as external interrupt?

ラベル(1)
3 返答(返信)

1,449件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Mar Kon

Q1. May I activate interrupt on every port A, B, C, D, E?

A1: No, Kinetis L series does not support all ports interrupt.

Q2. May I wake up processor with the use of external pin (for instance PTC6) and than use this pin as external interrupt?

A2: You can reference chapter "Interrupt channel assignments" in reference manual. There is a table which tell you which port can support GPIO interrupt and which port can only support single interrupt.

Hope my reply can help you.

Best Regards

Paul

1,449件の閲覧回数
Markon
Contributor II

Thank you for your answer.

May I ask you about reference manual for MKL16Z64VLH4 because there isn't any connected with this processor on freescale webside?

0 件の賞賛
返信

1,449件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Mar Kon,

    Reference manual for MKL16Z64VLH4 will be recently launched, please pay aattention to the website.

    Best regards!

Jing