For the KL03 in QFN pkg., should the center pad be grounded?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

For the KL03 in QFN pkg., should the center pad be grounded?

跳至解决方案
2,110 次查看
brenconsult
Contributor II

The datasheet doesn't appear to address the question of how to handle the exposed center pad of the QFN packages for the KL03 MCUs.  Ground it?  Leave it floating?

Thanks,

Scott

标签 (1)
标记 (1)
1 解答
1,969 次查看
EarlOrlando
Senior Contributor II

Hello Scott,

I think that the Application Note AN1902​ is what you are looking for. It has relevant information regarding hardware considerations for the QFN packages. Please take a look specially in the section 4.2.2 Thermal/Electrical Pad Guidelines.

Best regards,

Earl Ramírez.

/* If this post answers your question please click the Correct Answer button. */

在原帖中查看解决方案

3 回复数
1,969 次查看
Stano
NXP Employee
NXP Employee

Hi Scott,

yes the exposed center pad has to be grounded.

Best Regards,

Stano.

1,969 次查看
brenconsult
Contributor II

Thank you!  Is this documented some place, and I just missed it?

Scott

0 项奖励
回复
1,970 次查看
EarlOrlando
Senior Contributor II

Hello Scott,

I think that the Application Note AN1902​ is what you are looking for. It has relevant information regarding hardware considerations for the QFN packages. Please take a look specially in the section 4.2.2 Thermal/Electrical Pad Guidelines.

Best regards,

Earl Ramírez.

/* If this post answers your question please click the Correct Answer button. */