Flexbus and Parallel NOR FLASH connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flexbus and Parallel NOR FLASH connection

1,550 次查看
NEIL4
Contributor II

Im interfacing MK64FX Flexbus config as (16bit multiplexed) with Parallel NOR flash SST39VF802C which is Word(16bit) programmed.(With Ref AN4393)

The Parallel NOR flash has Address lines(0-18).

Which type of latch should you recommend and what should be the hardware connection.

 

0 项奖励
回复
2 回复数

1,539 次查看
jingpan
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,387 次查看
NEIL4
Contributor II

Capture.PNG

I have interfaced 16bit NOR flash(SST39LF802C) with MK64 via Latch (54ABT16373A), the connections are made as per the above diagram. Programming had done as per App. Note(AN4393).

During read, write and erase, the OE and R/W# are always at HIGH logic state. Due to which could not able to perform any operation on the flash. Any feedback is really helpful. Thank you!

 

 

0 项奖励
回复