FlexCan Kinetis K70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexCan Kinetis K70

5,535 Views
gaetanoanania
Contributor III

Hi All,

I'm looking for an application note about the flexcan. I am not interesting on the example , I just want to understand how can change and set the main registers.

I saw the examples made by freescale for other but very similar microcontroller ( for example k60) but they don't have any notes about the implementantion.

Can someone help me?

Thanks

Labels (1)
0 Kudos
Reply
7 Replies

3,890 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Please check attached file, which is Kinetis FlexCAN module training material with detailed info about Kinetis FlexCAN module.

Wish it helps.

3,890 Views
gaetanoanania
Contributor III

Hi Hui_Ma,

my TWR k70 at moment work fine at different baude rate from 83,3 k to 250 k with two clock reference ( 60 Mhz generated from PLL0 and 50 Mhz generated from external clock). I tryed to set the baud rate at 500k and 1M but the communication gets always errors.

I know the PLL clock has problem at high baud rate( tolerance problem) but using  the external clock I should solve it.

Below you can see the register setting for two different baud rate 125k and 250 k respectively using as clock reference the external clock at 50 MHz:

125 K 50Mhz:

50M/50= 1M sclock,

1M/125k= 8Tq

PROPSEG = 2, RJW = 2, PSEG1 = 2, PSEG2 =2, PRESDIV = 50

So the register setting becames:

            pFlexCANReg->CT2L1 = (0 | FLEXCAN_CTRL_PROPSEG(1)

           | FLEXCAN_CTRL_RJW(1)

           | FLEXCAN_CTRL_PSEG1(1)

           | FLEXCAN_CTRL_PSEG2(2)

           | FLEXCAN_CTRL_PRESDIV(49));        

And

250 K 50Mhz:

50M/25= 2M sclock,

2M/250k= 8Tq

PROPSEG = 2  RJW = 1, PSEG1 = 2, PSEG2 =3, PRESDIV =2 4

So the register setting becames:

pFlexCANReg->CTRL1 = (0 | FLEXCAN_CTRL_PROPSEG(1)

| FLEXCAN_CTRL_RJW(1)

         | FLEXCAN_CTRL_PSEG1(1)

| FLEXCAN_CTRL_PSEG2(2)

         | FLEXCAN_CTRL_PRESDIV(24));  


Using the same concepts if I tryed to set at 500 or 1000k with 50Mhz (external clock) the communication would get only faults .


Below the register setting:


                    ** 50M/10= 5M sclock,

                5M/500k=10Tq

          ** PROPSEG = 3

  ** RJW = 2, PSEG1 = 3, PSEG2 =3, PRESDIV = 10

          */

       /*   pFlexCANReg->CTRL1 = (0 | FLEXCAN_CTRL_PROPSEG(2)

| FLEXCAN_CTRL_RJW(2)

         | FLEXCAN_CTRL_PSEG1(2)

| FLEXCAN_CTRL_PSEG2(2)

         | FLEXCAN_CTRL_PRESDIV(9));






  Do you have any suggests? Or any register setting  that work fine?

Thanks in advance.


G.

0 Kudos
Reply

3,890 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

You can use Processor Expert tool to auto config FlexCAN bit rate.

I attached a project for your reference, the project based on CodeWarrior for MCU V10.5

Below picture shows timing configure picture for some detailed info:

FlexCAN setting.jpg

Wish it helps.

0 Kudos
Reply

3,890 Views
gaetanoanania
Contributor III

Hi ,

I was able to set up a can communication in loop_mode( k70 sends and receives the same data enabling the loop_mode bit). Now I want to send message from k70 and visualize it with an oscilloscope or signal analyzer.  My k70 is the only node of the bus and obviously it doesn't receive any ACK. In that configuration it sends always the same message ( because not receive ACK).

So, my question is :

Is there a way to avoid this problem and to send the message just when I want to send ( not continuously)? 

Or otherwise, Is there a way to avoid that the k70 sends again the message?

Thanks in advance.

G.

0 Kudos
Reply

3,890 Views
gaetanoanania
Contributor III

Hi Hui_Ma,

your document will be very useful for my work.

Thank you very much.

Regards.

Gaetano

0 Kudos
Reply

3,890 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Gaetano Anania,

    I think , you can according to the chapter of flexcan in reference manual, it describe flexcan in details.

   By the way, in our www.freescale.com, I find this link about can: http://www.freescale.com/webapp/sps/site/application.jsp?code=APLCAN

   And, there are some documents, maybe is useful to you!

I wish it helps you!

Best regards!

Jing

3,890 Views
gaetanoanania
Contributor III

Hi Jing,

thank you for your help. I 'll take you known about the improvment of my work...and I hope to have good news :-) !!!!

Regards.

Gaetano

0 Kudos
Reply