FlexBus for Intel 8080 parallel bus transfers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FlexBus for Intel 8080 parallel bus transfers

1,720 次查看
guenter_loettrich
NXP Employee
NXP Employee

Hi everyone,

is somebody aware of an example code and circuit diagram that uses FlexBus (on K22) for emulating the Intel 8080 parallel bus implementation (separate Read and Write signals)?

Thanks a lot in advance.

Guenter

2 回复数

1,097 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Guenter,

Please check the attachment.

The attachment is a FlexBus_LCD demo, the K22 control the LCD by using the Flexbus module.

2015-12-17_10-53-47.jpg


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,097 次查看
guenter_loettrich
NXP Employee
NXP Employee

Hi Ping,

thanks! This goes in the right direction. The speciality is that on Intel 8080 you have separate read and write signals (unlike on Motorola 6800 where a single R/W signal is used).

I don't know if anybody has ever worked on a solution with FlexBus to interface it to Intel 8080 bus with or without external logic.

br

Guenter

0 项奖励
回复