FlexBus K64 with MRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FlexBus K64 with MRAM

跳至解决方案
1,226 次查看
fshah30
Contributor II

Hello, I am interfacing MCU K64FN1M0VLQ12 with MRAM MR2A16ACMA35. 

1- Multiplex mode or non multiplex mode is fast?

2- In Multiplex mode, 16bit address and 16bit data, what are the connections required between MCU and MRAM?

0 项奖励
回复
1 解答
1,215 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @fshah30 ,

1. They are same.

2. FB_AD[1:18] <=Latch=>A[0:17];

    FB_AD[0:15]<==>D[0:15]

    ALE <->Latch ALE

    MRAM UB&LB can connect to ground.

   You can refer to AN4393 for other pins.

 

Regards,

Jing 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,216 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @fshah30 ,

1. They are same.

2. FB_AD[1:18] <=Latch=>A[0:17];

    FB_AD[0:15]<==>D[0:15]

    ALE <->Latch ALE

    MRAM UB&LB can connect to ground.

   You can refer to AN4393 for other pins.

 

Regards,

Jing 

0 项奖励
回复