Hi Sarathkumar S,
We seldom use Rowley cross works IDE, we normally use the MCUXpresso IDE, IAR or MDK.
So, we suggest you also use the above three IDE, this is the popular IDE.
After you modify the FSEC, you can generate the .hex file, then check flash address 0x0_040C, whether it is 0x00 which you defined?
Just check whether you IDE can generate the correct secured app .HEX file at first.
If you still have question about it, please kindly let me know.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------