Firmware for K20 of TWR-KV11Z75M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Firmware for K20 of TWR-KV11Z75M

1,194件の閲覧回数
lucagirotti
Contributor I

Hello, I have a TWR-KV11Z75M and I can't load any Open SDA Application because the bootloader doesn't work anymore (by pusshing the reset button and plugging the usb cable). I need to re-program the K20 through the JTAG port (J513 on the TWR board). Where can I find the binary file for the K20?

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,050件の閲覧回数
BlackNight
NXP Employee
NXP Employee

OpenSDA firmware files are listed here:

OpenSDA Serial and Debug Adapter|NXP 

I hope this helps,

Erich

0 件の賞賛
返信

1,050件の閲覧回数
lucagirotti
Contributor I

Exactly! Thank you Erich

0 件の賞賛
返信