Firmware for K20 of TWR-KV11Z75M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Firmware for K20 of TWR-KV11Z75M

732 Views
lucagirotti
Contributor I

Hello, I have a TWR-KV11Z75M and I can't load any Open SDA Application because the bootloader doesn't work anymore (by pusshing the reset button and plugging the usb cable). I need to re-program the K20 through the JTAG port (J513 on the TWR board). Where can I find the binary file for the K20?

0 Kudos
Reply
2 Replies

588 Views
BlackNight
NXP Employee
NXP Employee

OpenSDA firmware files are listed here:

OpenSDA Serial and Debug Adapter|NXP 

I hope this helps,

Erich

0 Kudos
Reply

588 Views
lucagirotti
Contributor I

Exactly! Thank you Erich

0 Kudos
Reply