Hello,I ask if it is possible on a K70 processor, you can use the firmware via an external FLASH.The Indoor 1 Mbyte space is almost finished. If I need more space as I do?
Maurizio Felicioni
Hi
If your external Flash is parallel and memory mapped on the FlexBus it can be used for program code.
Often external SDRAM is also used (faster) to run code from, after copying it there for a cheaper serial Flash, or NAND flash device.
Regards
Mark
hi,
I am using TWR K70 with external ddr2 ram.I could put my firmware in a serial flash, and then copy it into RAM?Is there any example?
Thank you very much
Maurizio