Hello all,
currently I'm trying to port an application from a MC56F847 controller to a Kinetis V4x controller. Therefore I need and an FTM counter to start counting based on an the beginning of an PWM cycle / signal. After two configureable delays I need to enable two outputs (independently).
So here is my concept so far:
- PWM generation: PWMA_0A -> PWMA0_TRG0
- Connection between PWM & FTM component: PWMA_A0_TRG0 -> over xbar -> FTM0_TRIG2
- Two channels as output compar mode: FTM0_CH0 & FTM0_CH1
I use the following code o initializ the timer component:
ftmConfig.extTriggers =kFTM_Chnl0Trigger;
ftmConfig.chnlInitState =0;
ftmConfig.pwmSyncMode =kFTM_HardwareTrigger_2;
if (FTM_Init(FTM0, &ftmConfig) != kStatus_Success)
{
return false;
}
FTM_SetupOutputCompare(FTM0, kFTM_Chnl_0, kFTM_SetOnMatch, 1000);
FTM0->SYNC |= (1<<2); // reinit
FTM0->CNTIN =0U;
FTM0->MOD =0xFFFFU;
And here the problem begins. If I now enable the timer via FTM_StartTimer(...) it starts counting and the channel 0 output will be set after a while. Is it possible start the counting when the signal TRIG2 occurs? The other problem is, that the counter currently just overflows and starts counting from zero again - but it should stop counting and reset the outputs to their initial values - is that possible?
Best Regards,
Florian
解決済! 解決策の投稿を見る。
Hello XiangJun,
thanks again for your fast response. After changing the trigger signal as explained the synchronization wasn't working (xbarin-xbarout34 and the direct soultion (pwma0_trig0 - xbarout34)). After reading the reference manual again and again I have found the comment "only the enhanced PWM synchronization must be used" - so my gues is that the legacy PWM mode shouldn't be used on this device right? I have changed the corresponding bit in the SYSCONF register and now its working. I have attached the working code - if someone else will have the same issue in the future....
Best Regards,
Florian
<CODE>
CLOCK_EnableClock(kCLOCK_PortC);
CLOCK_EnableClock(kCLOCK_Ftm0);
PORT_SetPinMux(PORTC, 1u, kPORT_MuxAlt4); // FTM0_CH0 on PTC1
PORT_SetPinMux(PORTC, 2u, kPORT_MuxAlt4); // FTM0_CH1 on PTC2
XBARA_SetSignalsConnection(XBARA, kXBARA_InputPwm0Trg0, kXBARA_OutputFtm0Trig2); // connect kXBARA_InputPwm0Trg0 to kXBARA_OutputFtm0Trig2
// configure hardware trigger
SIM->SOPT4 |= (SIM_SOPT4_FTM0TRG2SRC_MASK);
FTM0->SYNC |= 0x40; // enable hw trigger 2
FTM0->SYNCONF |= 0x30081;
// configure PWM on FTM0_CH0/1 (PTC1/2)
FTM0->CONF=0xC0; //set up BDM in 11
FTM0->FMS=0x00; //clear the WPEN so that WPDIS is set in FTM0_MODE reg
FTM0->MODE|=0x05; //enable write the FTM CnV register
FTM0->MOD=2000;
FTM0->CONTROLS[0].CnSC=0x28; //High_Low_High for center-alignment
FTM0->CONTROLS[1].CnSC=0x28; //High_Low_High for center-alignment
FTM0->COMBINE|=0x20; //enable update the FTM_C0V/FTM0_C1V register
FTM0->COMBINE|=0x02; //complementary mode for CH0&CH1 of FTM0
FTM0->COMBINE|=0x10; // dead timer insertion enabled in complementary mode for //CH0&CH1 of
FTM0->DEADTIME=0x00; //dead time is 0 system clock cycles
FTM0->CONTROLS[1].CnV=500;
FTM0->CONTROLS[0].CnV=500;
FTM0->CNTIN=0x00;
FTM0->SC=0x08; // system clock driving, dividing by 1
</CODE>
i think counter will count till MOD value. In this case MOD is 0xFFFF so it will count till max value. try changing MOD value to your desired value
Hello sumit,
thanks for your response but the overflow itself isn't the problem - the hardware trigger doesn't work as expected which should reset the counter long time before the overlfow happens.
Best Regards,
Florian
Hi, Florian,
I think your solution is okay.
You have the PWMA_0A triggering signals(XBARA_IN20 or PWMA0_TRG0) route to FTM0_TRIG2(XBARA_OUT34) via crossbar, and use the FTM0_TRIG2 to synchronize FTM0 counter. You can set the FTM0 MOD register as the maximum value 0xFFFF, when the FTM0_TRIG2 signal arrives, the FTM counter FTM0_CNT register is initialized by the FTM0_CNTIN register, the FTM0_CNT will begin to count from the FTM0_CNTIN value. The FTM_StartTimer(...) function only sets the CLKS bits in FTM0_SC register so that the FTM0_CNT begins to count. As I said the FTM0_CNT will be initialized with FTM0_CNTIN value when the rising edge of FTM0_TRIG2 comes.
I suggest you refer to an5142, which has the code for hardware triggering.
BR
XiangJun Rong
Hello XiangJun,
thanks for your fast response. I have tried the exmaple in chapter 3.11.4 (Updating the FTM register with hardware control) which was the base for my previous tests. I have used the code from the application note with only one change - I have to use FTM0_FLT1 instead of FTM0_FLT0. I can't get the example running...I have also attached the a screenshot of the signals. The yellow one show the input signal of FTM0_FLT1 (GC0) and the green one show the signal of PTC1 - you can see that the rising edge of the yellow signal is ignored by the timer component. Any suggestions / ideas?
Best Regards,
Florian
<CODE>
CLOCK_EnableClock(kCLOCK_PortC);
CLOCK_EnableClock(kCLOCK_Ftm0);
PORT_SetPinMux(PORTC, 0u, kPORT_MuxAlt6); // FTM0_FLT1 (alt6) on PTC0
PORT_SetPinMux(PORTC, 1u, kPORT_MuxAlt4); // FTM0_CH0 on PTC1
PORT_SetPinMux(PORTC, 2u, kPORT_MuxAlt4); // FTM0_CH1 on PTC2
// configure hardware trigger
SIM->SOPT4 &=~(SIM_SOPT4_FTM0FLT1_MASK);
FTM0->SYNC |= 0x40; // enable hw trigger 2
FTM0->SYNCONF |= 0x30001;
// configure PWM on FTM0_CH0/1 (PTC1/2)
FTM0->CONF=0xC0; //set up BDM in 11
FTM0->FMS=0x00; //clear the WPEN so that WPDIS is set in FTM0_MODE reg
FTM0->MODE|=0x05; //enable write the FTM CnV register
FTM0->MOD=1000;
FTM0->CONTROLS[0].CnSC=0x28; //High_Low_High for center-alignment
FTM0->CONTROLS[1].CnSC=0x28; //High_Low_High for center-alignment
FTM0->COMBINE|=0x20; //enable update the FTM_C0V/FTM0_C1V register
FTM0->COMBINE|=0x02; //complementary mode for CH0&CH1 of FTM0
FTM0->COMBINE|=0x10; // dead timer insertion enabled in complementary mode for //CH0&CH1 of
FTM0->DEADTIME=0x00; //dead time is 0 system clock cycles
FTM0->CONTROLS[1].CnV=500;
FTM0->CONTROLS[0].CnV=500;
FTM0->CNTIN=0x00;
FTM0->SC=0x28; //PWM center_alignment, system clock driving, dividing by 1
</CODE>
Hi, Florian,
I suppose that you can NOT use FTM0_FLT1(PTC0) as hardware triggering signal. Pls refer to sectin 39.1.6 FTM Hardware Triggers in the reference manual of KV4x, only XBARA_OUT34 can be used as FTM0 hardware triggering source2. If you want to use external signal as FTM0 hardware triggering source2, you can connect the signal to any XB_INx pin and route the signal to XBARA_OUT34.
for example, you can connect the external triggering signal to PTC5/XBAR0_IN2
CLOCK_EnableClock(kCLOCK_PortC);
PORT_SetPinMux(PORTC, 5u, kPORT_MuxAlt4); //PTC5 as XBAR0_IN2/ALT4
XBARA_SEL17&=~(0x3F);
XBARA_SEL17|=0x02; //route the XBAR0_IN2 to XBARA_OUT34.
If you use the PWMA_0A triggering signal
XBARA_SEL17&=~(0x3F);
XBARA_SEL17|=20; //route the PWMA0_TRG0 to XBARA_OUT34.
Hope it can help you
BR
Xiangjun Rong
Hello XiangJun,
thanks again for your fast response. After changing the trigger signal as explained the synchronization wasn't working (xbarin-xbarout34 and the direct soultion (pwma0_trig0 - xbarout34)). After reading the reference manual again and again I have found the comment "only the enhanced PWM synchronization must be used" - so my gues is that the legacy PWM mode shouldn't be used on this device right? I have changed the corresponding bit in the SYSCONF register and now its working. I have attached the working code - if someone else will have the same issue in the future....
Best Regards,
Florian
<CODE>
CLOCK_EnableClock(kCLOCK_PortC);
CLOCK_EnableClock(kCLOCK_Ftm0);
PORT_SetPinMux(PORTC, 1u, kPORT_MuxAlt4); // FTM0_CH0 on PTC1
PORT_SetPinMux(PORTC, 2u, kPORT_MuxAlt4); // FTM0_CH1 on PTC2
XBARA_SetSignalsConnection(XBARA, kXBARA_InputPwm0Trg0, kXBARA_OutputFtm0Trig2); // connect kXBARA_InputPwm0Trg0 to kXBARA_OutputFtm0Trig2
// configure hardware trigger
SIM->SOPT4 |= (SIM_SOPT4_FTM0TRG2SRC_MASK);
FTM0->SYNC |= 0x40; // enable hw trigger 2
FTM0->SYNCONF |= 0x30081;
// configure PWM on FTM0_CH0/1 (PTC1/2)
FTM0->CONF=0xC0; //set up BDM in 11
FTM0->FMS=0x00; //clear the WPEN so that WPDIS is set in FTM0_MODE reg
FTM0->MODE|=0x05; //enable write the FTM CnV register
FTM0->MOD=2000;
FTM0->CONTROLS[0].CnSC=0x28; //High_Low_High for center-alignment
FTM0->CONTROLS[1].CnSC=0x28; //High_Low_High for center-alignment
FTM0->COMBINE|=0x20; //enable update the FTM_C0V/FTM0_C1V register
FTM0->COMBINE|=0x02; //complementary mode for CH0&CH1 of FTM0
FTM0->COMBINE|=0x10; // dead timer insertion enabled in complementary mode for //CH0&CH1 of
FTM0->DEADTIME=0x00; //dead time is 0 system clock cycles
FTM0->CONTROLS[1].CnV=500;
FTM0->CONTROLS[0].CnV=500;
FTM0->CNTIN=0x00;
FTM0->SC=0x08; // system clock driving, dividing by 1
</CODE>