FTM Fault Detection Inputs in KV31

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTM Fault Detection Inputs in KV31

1,077件の閲覧回数
soerenbirth
Contributor I

ChipConfigurationFTMFaults.PNGSIMSOPT_Bits.PNG

Hey there,

i have a  question about FTM Fault in MKV31F512VLL12 reference manual. As depicted above the chip configuration chapter has more fault detection input than the SIM_SOPT4 has bits for. Which one is correct?

Best regards

Sören

0 件の賞賛
返信
1 返信

927件の閲覧回数
marekzeman-b508
NXP Employee
NXP Employee

Hello Sören,

I suppose that both chapters are correct, because in SIM_SOPT4 register you can choose fault detection input between two possible options (fault pin or CMP), for example FTM1_FAULT0.

Even, FTM1_FAULT1 is hardwired to CMP1 output, thus, you are not able to change Fault input. There is not required changes in register.

best regards,

M.

0 件の賞賛
返信