FTFA fails erasing flash, frdm kl43

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTFA fails erasing flash, frdm kl43

ソリューションへジャンプ
2,634件の閲覧回数
alexeyusoltsev
Contributor IV

HI!

I am trying to save some data to Flash. For practice I am using frdm kl43 board but the final product will be on kv10. So the decision not to use FlexNVM functionality but ordinary flash module functionality. I am trying to follow example but with PE. My main and PE is here:

116749_116749.jpgmain.jpg

(main also attached)

Debugging the code i get to

Reset_Handler:

    cpsid   i               /* Mask interrupts

 

Best regards,

Alexey

Original Attachment has been moved to: main.c.zip

タグ(3)
0 件の賞賛
返信
1 解決策
2,258件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Alexey Usoltsev:

I guess this is caused by SysTick interrupt firing. The interrupt handler is in the same flash block and it leads to a "Read-while-write error".

- Try setting the OSA timer to None as discussed in the next thread:

Guidance on fsl_flash Processor Expert component usage

- Or enable the ESFC bit as explained in the next discussion:

Writing flash memory with KL27Z256

Let me know it the problem is not solved.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
2,259件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Alexey Usoltsev:

I guess this is caused by SysTick interrupt firing. The interrupt handler is in the same flash block and it leads to a "Read-while-write error".

- Try setting the OSA timer to None as discussed in the next thread:

Guidance on fsl_flash Processor Expert component usage

- Or enable the ESFC bit as explained in the next discussion:

Writing flash memory with KL27Z256

Let me know it the problem is not solved.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,258件の閲覧回数
alexeyusoltsev
Contributor IV

Hello again Jorge Gonzalez,

I am a bit confused a bit MCM_PLACAR ESFC bit.

I am setting ESFC bit by MCM_PLACR_ESFC(1); but if one let global interrupts be enabled it still fails. If interrupts are desabled erase-write goes "ok".

Regards,

Alexey.

0 件の賞賛
返信
2,258件の閲覧回数
alexeyusoltsev
Contributor IV

Hello Jorge Gonzalez,

It worked out!!! Many thanks. And the info about arbitration using is very helpful too!

0 件の賞賛
返信
2,258件の閲覧回数
alexeyusoltsev
Contributor IV

  I've launched example successfully. But in my programm when pressing F3 on erase function one can see error:

error.jpg

may be I have to compile C90TFS lib elsewhere?

0 件の賞賛
返信