FRDM-KW40Z with Test Tool 12

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-KW40Z with Test Tool 12

783 次查看
koonlee
Contributor I

I have a FRDM-KW40Z board and I would like to use Radio Test application in Test Tool 12.

First, I use Firmware Loaders to load "MAC 2003 ZTC 115200 KW24D512-USB ASP_RadioTest.srec".  I see "CMSIS-DAP MSD (E:\)" under the OpenSDA/J-Link List. When I click Upload button, I got the following error:

"Error: could not access MSD drive"

Did I miss any step?

Thanks for your help.

Koon

0 项奖励
回复
1 回复

436 次查看
isaacavila
NXP Employee
NXP Employee

Hello Koon,

Available images for Test tool are not compatible for KW40 MCU, as you can see, your image "MAC 2003 ZTC 115200 KW24D512-USB ASP_RadioTest.srec" is available for KW24D512 and not for KW40. So, you cannot use KW24's images to flash KW40 target.

Sorry for this inconvenience!

Regards,

Isaac Avila

0 项奖励
回复