Hi luis-martinez,
You are wrong, the J11 is used to disconnect the on board debugger to the on board KV31 target chip.
Then J11 can used as the debugger to program the external board.
So, if you just want to use the external debugger eg JLINK, you don't need to disconnect J11, you still need to connect J11, and connect your external debugger to J9. Just make sure the on board debugger is not the same as your external debugger.
If your on board is already opensda, then you can use your external JLINK as the debugger directly.
The on board R34 should be DNP, which is not connected.
You even don't need to modify the FRDM-KV31F, then you can use the external JLINK directly.
Please try it on your side.
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------