FRDM-KL26Z MCU in reset state

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL26Z MCU in reset state

1,192 Views
daewoong
Contributor I

Hello

I'm new in this MCU. I bought FRDM-KL26Z and connected Jlink by cutting SDA (J8 open). It was not successful. LED indicator of Jlink was saying "reset is active on the target". I checked the reset pin of target MCU. It was only 0.9V (/w and /wo Jlink connection). With this, I guess there is something wrong in the board hardware.

Below is the capture from MCUXpresso IDE.

Could you advise ?

Thanks and regards, Daewoong

daewoong_0-1612702108689.png

 

 

0 Kudos
Reply
1 Reply

1,188 Views
nxf58904
NXP Employee
NXP Employee

Hi,

Try as follows:

1.unplug board 

2.press "NMI"

3.plug-in

4.Download

 

0 Kudos
Reply