FRDM-KL25Z not giving 3v3 and also gets over heated on regulator side

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL25Z not giving 3v3 and also gets over heated on regulator side

459 Views
krishnakumargan
Contributor I

Dear Freescale engineers,

  In FRDM - KL25Z, Am driving Vin(input voltage) as 5volt. I am not able

to get 3.3v with reference to ground, instead of 3.3v am getting

2.2volt in 3v3 pinout, and also Voltage regulator and microcontroller

getting more hotter.

Thanks & Regards,

krishnakumar.G

Hetrogenous Communications Technologies Pvt Ltd.

No.25, Block - 2, 2 nd floor, SIDCO Indusrtrial Estate, Guindy,

Chennai - 600032.

cell : +91 - 9965899278

email : krishnakumar@hetrogenous.com

0 Kudos
1 Reply

340 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Krishnakumar,

Obviously, there's some errors with the board, then cause the voltage level drop.

And I'd like to confirm with you whether the board works in standalone mode or not when you measure the 3v3 voltage of the FRDM-KL25.

I've also checked my board on hand, it can supply 3.3v for MCU.

I'm looking forward to your reply.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos