FRDM-KEAZ128 can't connect to the S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KEAZ128 can't connect to the S32DS

Jump to solution
1,106 Views
elder_atom
Contributor II

At first ,FRDM-KEAZ128 can connect to the S32DS normally, then I drag a MSD-DEBUG-FRDMP-KEAZ128Q80_Pemicro_v118.SDA file to the board in the bootloader mode and when I download the project to the board ,I find the board can't connect to the S32DS.

Thank you!

窗口界面.PNG

Labels (1)
0 Kudos
Reply
1 Solution
971 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Li Yinwei ,

I use the same file to update the bootloader, it still can work well.

Please change to a new workspace through File ->Switch Workspace ,

then create a simple new project to have a try.

Also please check the Device Manager whether the board been detected.

BR

Alice

View solution in original post

0 Kudos
Reply
1 Reply
972 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Li Yinwei ,

I use the same file to update the bootloader, it still can work well.

Please change to a new workspace through File ->Switch Workspace ,

then create a simple new project to have a try.

Also please check the Device Manager whether the board been detected.

BR

Alice

0 Kudos
Reply