FRDM-K64F flashing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-K64F flashing

889 次查看
a8Chcx
Contributor V

Hi,

I bought the new FRDM-K64 boards with REV E .

I am trying to flash the program into board by using MCHXpresso IDE 11.5.0 and J9 and always got error to connect.

But, when I use the old board with REV C and everything works fine.

Can anyone tell me the difference between two boards?

Thanks,

 

Christie

0 项奖励
回复
3 回复数

857 次查看
a8Chcx
Contributor V

Hi Habib,

 Can you tell me where to get the latest document for REV E and SCH F1 because I follow your link to download the document and is not latest?

Thanks,

Christie

0 项奖励
回复

819 次查看
Habib_MS
NXP Employee
NXP Employee

Hello again @a8Chcx,


You can find the FRDM-K64F Schematics E4 version at the following link, in the window called "Design Files". Additionally, the only user's guide available for the FRDM-K64F is the one I provided to you.

BR
Habib

0 项奖励
回复

868 次查看
Habib_MS
NXP Employee
NXP Employee

Hello @a8Chcx,

The schematic includes detailed information about the modifications made to the board. For instance, the change log for the REV E4 schematic outlines these updates:

Habib_MS_1-1745966731309.png

In the other hand, I highly recommend see the Getting Started with the FRDM-K64F in order to obtain more information.


BR
Habib

0 项奖励
回复