FRDM K64F board hangs after 2 days when connected to network

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FRDM K64F board hangs after 2 days when connected to network

跳至解决方案
2,872 次查看
rahul_eris
Contributor II

Hi All,

          We are working on KSDK example demo project lwip-tcpecho demo.

Added our own additional threads for tcp ip communication for ports 4442(web application) and 80(web server).

Our implementations are depending more on heap memory rather than stack( Ensured proper freeing and deallocation after heap use).

Our problem is that when the board is connected to ethernet continuously it got hangs after 1, 2 days. Then we need to restart again .   It makes our product application a unusable one.

We tried out different cases for debugging the issue.

-We tried by stopping all other threads except web application but the problem exist.

-Ensured that different MAC ids are assigned for different boards.

-When disconnecting from ethernet, this problem is not seen.

We are suspecting the issue is with the lwip tcp ip stack porting. Not sure about this.

Can anybody suggest a better and needed solution for this.

Now we have got the assert while hanging   "pbuf_free: p->re..."

Thanks,

Rahul

标签 (1)
0 项奖励
回复
1 解答
2,121 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Rahul,

Thank you for the patience.

Please check below KSDK team feedback about this issue:

  There's a patch in KSDK1.3GA which might resolve this issue.

  [KPSDK-7362][LWIP]Fix the lwip rtos ping block issue

diff --git a/middleware/tcpip/lwip/port/ethernetif.c b/middleware/tcpip/lwip/port/ethernetif.c
index 6e63cd0..044b5bd 100644
--- a/middleware/tcpip/lwip/port/ethernetif.c
+++ b/middleware/tcpip/lwip/port/ethernetif.c
@@ -688,14 +688,13 @@ ethernetif_init(struct netif *netif)
#if defined(FSL_RTOS_MQX)
     OSA_InstallIntHandler(ENET_Transmit_IRQn, MQX_ENET_Transmit_IRQHandler);
     OSA_InstallIntHandler(ENET_Receive_IRQn, MQX_ENET_Receive_IRQHandler);
-#if defined(FSL_RTOS_MQX)
     OSA_InstallIntHandler(ENET_1588_Timer_IRQn, MQX_ENET_1588_Timer_IRQHandler);
#endif
   /* Set priority for ISRs */
   NVIC_SetPriority(ENET_1588_Timer_IRQn, 4U);
-  NVIC_SetPriority(ENET_Transmit_IRQn, 4U);
-  NVIC_SetPriority(ENET_Receive_IRQn, 4U);
-#endif
+  NVIC_SetPriority(ENET_Transmit_IRQn, 5U);
+  NVIC_SetPriority(ENET_Receive_IRQn, 5U);
+
   /* initialize the hardware */
   result = low_level_init(netif);

diff --git a/middleware/tcpip/lwip/port/lwipopts.h b/middleware/tcpip/lwip/port/lwipopts.h
index 199d0f0..dde8b8a 100644
--- a/middleware/tcpip/lwip/port/lwipopts.h
+++ b/middleware/tcpip/lwip/port/lwipopts.h
@@ -37,14 +37,14 @@
#define __LWIPOPTS_H__
/*include fsl os abstraction header file to judge whether OS is used*/
#include "fsl_os_abstraction.h"
+
+#if USE_RTOS
/**
  * SYS_LIGHTWEIGHT_PROT==1: if you want inter-task protection for certain
  * critical regions during buffer allocation, deallocation and memory
  * allocation and deallocation.
  */
-#define SYS_LIGHTWEIGHT_PROT    0
-#if USE_RTOS
-

+#define SYS_LIGHTWEIGHT_PROT    1

/**

  * NO_SYS==0: Use RTOS

  */

  In KSDK1.2GA, the SYS_LIGHTWEIGHT_PROT  macro is not enabled when RTOS is used, which may lead to crash for global variable is not protected.

I would recommend customer to update software to latest KSDK software.

You could find the latest KDSK software from below link:

Welcome to Kinetis Expert | Kinetis Expert


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

5 回复数
2,121 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Rahul,

Please provide the KSDK software version you are using. Thanks.

best regards,

Ma Hui

0 项奖励
回复
2,121 次查看
rahul_eris
Contributor II

We are using Ksdk 1.2.0 and KDS 3.0.0.

Using the example project lwip tcpecho example for mqx in frdmk64f

Now we are getting the lwip assert as "tcpip_thread: invalid message:" on crash.

thanks

Rahul

0 项奖励
回复
2,122 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Rahul,

Thank you for the patience.

Please check below KSDK team feedback about this issue:

  There's a patch in KSDK1.3GA which might resolve this issue.

  [KPSDK-7362][LWIP]Fix the lwip rtos ping block issue

diff --git a/middleware/tcpip/lwip/port/ethernetif.c b/middleware/tcpip/lwip/port/ethernetif.c
index 6e63cd0..044b5bd 100644
--- a/middleware/tcpip/lwip/port/ethernetif.c
+++ b/middleware/tcpip/lwip/port/ethernetif.c
@@ -688,14 +688,13 @@ ethernetif_init(struct netif *netif)
#if defined(FSL_RTOS_MQX)
     OSA_InstallIntHandler(ENET_Transmit_IRQn, MQX_ENET_Transmit_IRQHandler);
     OSA_InstallIntHandler(ENET_Receive_IRQn, MQX_ENET_Receive_IRQHandler);
-#if defined(FSL_RTOS_MQX)
     OSA_InstallIntHandler(ENET_1588_Timer_IRQn, MQX_ENET_1588_Timer_IRQHandler);
#endif
   /* Set priority for ISRs */
   NVIC_SetPriority(ENET_1588_Timer_IRQn, 4U);
-  NVIC_SetPriority(ENET_Transmit_IRQn, 4U);
-  NVIC_SetPriority(ENET_Receive_IRQn, 4U);
-#endif
+  NVIC_SetPriority(ENET_Transmit_IRQn, 5U);
+  NVIC_SetPriority(ENET_Receive_IRQn, 5U);
+
   /* initialize the hardware */
   result = low_level_init(netif);

diff --git a/middleware/tcpip/lwip/port/lwipopts.h b/middleware/tcpip/lwip/port/lwipopts.h
index 199d0f0..dde8b8a 100644
--- a/middleware/tcpip/lwip/port/lwipopts.h
+++ b/middleware/tcpip/lwip/port/lwipopts.h
@@ -37,14 +37,14 @@
#define __LWIPOPTS_H__
/*include fsl os abstraction header file to judge whether OS is used*/
#include "fsl_os_abstraction.h"
+
+#if USE_RTOS
/**
  * SYS_LIGHTWEIGHT_PROT==1: if you want inter-task protection for certain
  * critical regions during buffer allocation, deallocation and memory
  * allocation and deallocation.
  */
-#define SYS_LIGHTWEIGHT_PROT    0
-#if USE_RTOS
-

+#define SYS_LIGHTWEIGHT_PROT    1

/**

  * NO_SYS==0: Use RTOS

  */

  In KSDK1.2GA, the SYS_LIGHTWEIGHT_PROT  macro is not enabled when RTOS is used, which may lead to crash for global variable is not protected.

I would recommend customer to update software to latest KSDK software.

You could find the latest KDSK software from below link:

Welcome to Kinetis Expert | Kinetis Expert


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,121 次查看
rahul_eris
Contributor II

Thanks Ma Hui and KSDK team for the support.

The issue solved by defining   SYS_LIGHTWEIGHT_PROT  to  1

0 项奖励
回复
2,121 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Rahul,

I am checking with Kinetis application team about this issue.

I will let you know when there with any feedback. Thank you for the patience.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复