FRDM-K64F Revision E3 not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K64F Revision E3 not working

Jump to solution
1,518 Views
intertronic
Contributor II

Hi everyone,

we are using two different versions (D1 and E3) of the FRDM-K64.

Booth are loaded with OpenSDA V2 and we use the KDS 3.

But with the E3 the usb-connection/debugging with the desktop is not stable. Sometimes it runs for 20 minutes, sometimes it hangs after 3 steps.

Does anybode else has such problems?

Regards

0 Kudos
Reply
1 Solution
1,378 Views
ivadorazinova
NXP Employee
NXP Employee

Hello intertronic,

please, have you tried to reload open sda firmware on the FRDM-K64F ?

On my side is running FRDM-K64F - schematic E3 revision without some problems.

In other case, is it possible for you to attach screen of the error?

Best Regards,

Iva

View solution in original post

0 Kudos
Reply
2 Replies
1,379 Views
ivadorazinova
NXP Employee
NXP Employee

Hello intertronic,

please, have you tried to reload open sda firmware on the FRDM-K64F ?

On my side is running FRDM-K64F - schematic E3 revision without some problems.

In other case, is it possible for you to attach screen of the error?

Best Regards,

Iva

0 Kudos
Reply
1,378 Views
intertronic
Contributor II

Hello Iva,

Problem seems to be solved.

The problem was, that the USB seems to break down. We used the OpenSDA

version 2 with a version from last year which was working with the old

FRDM-K64F. further we used the version 2015-04-23 which doesn't work. We

found a new version 2015-06-11 which is working with the new FRDM-K64F...

Thanks, Josef

Am 14.07.2015 15:02, schrieb ivadorazinova:

>

Freescale Community

<http://jiveon.jivesoftware.com/mpss/c/owA/PDcDAA/t.1op/Wd4oS6ZkS1a4b3kVkvPiiA/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

<http://jiveon.jivesoftware.com/mpss/c/owA/PDcDAA/t.1op/Wd4oS6ZkS1a4b3kVkvPiiA/h0/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bQ-3D>

>

FRDM-K64F Revision E3 not working

reply from Iva Dorazinova

<http://jiveon.jivesoftware.com/mpss/c/owA/PDcDAA/t.1op/Wd4oS6ZkS1a4b3kVkvPiiA/h1/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bTV2H6l88qkV2k9D4HQo1uUWCFUeozZRGYbPu5sDFrZDsGKUic9H-2BaheNxdnhWEhJU-3D>

in /Kinetis Microcontrollers/ - View the full discussion

<http://jiveon.jivesoftware.com/mpss/c/owA/PDcDAA/t.1op/Wd4oS6ZkS1a4b3kVkvPiiA/h2/eqhG5v9o4WV1pCmWaB03cUjBPgRj-2F3GoJUaXSZ409bSDdtwb8JVqMb8Sn4bht2-2FbBJDAxvikVF8Q-2F1HzqGadvABOgc1joeLdeDal0dJRJDw-3D>

>

0 Kudos
Reply