FRDM-K22F openSDA option doesn't appear on CW10.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K22F openSDA option doesn't appear on CW10.6

917 Views
josealonsovalle
Contributor III

Hi everyone,

i am trying to create a project in CW 10.6 with the FRDM board K22F-120Mhz, but in the connections window doesn't appear the OpenSDA option, what means this?, beacuse i already installed the firmware to the openSDA at the frdm, and  i have been working properly with the FRDM KL25Z and this board works good. , or, am i forced to use the Kinetis design studio to work with the K22F frdm board??,

Can somebody help me please??

i am not shure which of these MCU i must select, but however any of the boards haven't the option openSDA..

1.PNG.png

2.PNG.png

Labels (1)
0 Kudos
Reply
1 Reply

791 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Alonso:

This question is repeated. Please check response in the CodeWarrior thread:

FRDM-K22F openSDA option doesn't appear on CW10.6

Regards!

Jorge Gonzalez

0 Kudos
Reply