FOC function in KV4x or KV5x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FOC function in KV4x or KV5x

跳至解决方案
1,412 次查看
deega_jung
Contributor III

Hi NXP,

Could you advice me about the FOC, below is a project inform.

Application : ESC Drone 

Require spec.

Supply Voltage : 48V

Current : 60A

Motor Control Concept : PWM Speed Control and Sensorless FOC Control

 

Please let me know if your KV4x or KV5x solution supports sensorless FOC function for motor control.

If not supported, please let me know which product is a solution that supports sensorless FOC and PWM speed control with the above specifications.

Thanks,

Deega

0 项奖励
回复
1 解答
1,399 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Deega,

If you are interested on the KV family for your implementation, Application Note 5237 (AN5237, link below) may be of use as a starting point for your own motor control application.

https://www.nxp.com/docs/en/application-note/AN5237.pdf

I hope that this information helps.

Regards,
Gustavo

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,400 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Deega,

If you are interested on the KV family for your implementation, Application Note 5237 (AN5237, link below) may be of use as a starting point for your own motor control application.

https://www.nxp.com/docs/en/application-note/AN5237.pdf

I hope that this information helps.

Regards,
Gustavo

0 项奖励
回复
1,387 次查看
deega_jung
Contributor III

Hello Gustavo,

Thank you for your reply, there's a lot of help.

Thanks,

Deega

0 项奖励
回复