External Flash tool for Kinetis MCUs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

External Flash tool for Kinetis MCUs

跳至解决方案
2,019 次查看
darnaiadam
Contributor III

Hi,

I'm interested about flash my freedom board with an external tool, instead of internal Eclipse Flash programmer. Is there any way to do it? (OS is Linux Ubuntu)

标记 (2)
1 解答
1,821 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Darnai Adam,

I think the JLink tool is good choice.

And you can learn the more information about the Eclipse with GDB through the thread below.

https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/ 


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

5 回复数
1,821 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Darnai Adam,

To be honest, I'm not very clear the meaning of the internal Eclipse Flash programmer you mentioned above.

So can you explain it again? And do you want some debug tools?
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,821 次查看
bcamp
Contributor III

Hi

I suspect that:

Eclipse = KDS supplied / bundled programmer.

External = stand alone programmer that will load the same files without KDS being installed.

Bob

1,821 次查看
darnaiadam
Contributor III

Yes, thats what I meant. I'd like to use a programmer that communicates with GDB server and than flash my application through the USB connection to the Processor, without any IDE, for example KDS. I read that there are solutions via terminal, but I prefer an application that provide a GUI for the user.

0 项奖励
回复
1,822 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Darnai Adam,

I think the JLink tool is good choice.

And you can learn the more information about the Eclipse with GDB through the thread below.

https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/ 


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,821 次查看
darnaiadam
Contributor III

Thank you very much!

0 项奖励
回复