External Flash tool for Kinetis MCUs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External Flash tool for Kinetis MCUs

ソリューションへジャンプ
3,698件の閲覧回数
darnaiadam
Contributor III

Hi,

I'm interested about flash my freedom board with an external tool, instead of internal Eclipse Flash programmer. Is there any way to do it? (OS is Linux Ubuntu)

タグ(2)
1 解決策
3,500件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Darnai Adam,

I think the JLink tool is good choice.

And you can learn the more information about the Eclipse with GDB through the thread below.

https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/ 


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
3,500件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Darnai Adam,

To be honest, I'm not very clear the meaning of the internal Eclipse Flash programmer you mentioned above.

So can you explain it again? And do you want some debug tools?
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,500件の閲覧回数
bcamp
Contributor III

Hi

I suspect that:

Eclipse = KDS supplied / bundled programmer.

External = stand alone programmer that will load the same files without KDS being installed.

Bob

3,500件の閲覧回数
darnaiadam
Contributor III

Yes, thats what I meant. I'd like to use a programmer that communicates with GDB server and than flash my application through the USB connection to the Processor, without any IDE, for example KDS. I read that there are solutions via terminal, but I prefer an application that provide a GUI for the user.

0 件の賞賛
返信
3,501件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Darnai Adam,

I think the JLink tool is good choice.

And you can learn the more information about the Eclipse with GDB through the thread below.

https://mcuoneclipse.com/2015/03/25/command-line-programming-and-debugging-with-gdb/ 


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,500件の閲覧回数
darnaiadam
Contributor III

Thank you very much!

0 件の賞賛
返信