Ethernet flashing FRDM-K64F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Ethernet flashing FRDM-K64F

1,346 Views
miguelgonzalez
Contributor II

Hi.

Is there a way to update the flash program sending the binary file (.bin) by ethernet?

I am using a FRDM-K64F.

Thanks.

0 Kudos
Reply
2 Replies

1,138 Views
fangli
NXP Employee
NXP Employee

Hi,

Yes. Please download the FNET software from below link, which provides Ethernet bootloader for K64 product: http://fnet.sourceforge.net/

0 Kudos
Reply

1,139 Views
mjbcswitzerland
Specialist V

Hi

There are also Ethernet boot-loaders for the FRDM-K64F in the uTasker project:
http://www.utasker.com/kinetis/FRDM-K64F.html
With 30.9k Flash you can also have one that does Ethernet Web Server, USB-MSD, KBOOT-USB-HID and UART SREC loading all at the same time....

Regards

Mark

Open source at http://www.utasker.com/kinetis.html

0 Kudos
Reply