Ethernet clock configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Ethernet clock configuration

跳至解决方案
1,610 次查看
marcoantoniodeo
Contributor II

Hi all,

 

I have an year long project using KDS_v3 , KSDK_1.3.0 and Processor Expert. I know support ended for PE, but I want to ask a few questions:

 

  1. How is the minimum clock frequency configuration for the Ethernet work, in the means of mode, core clock, flash etc?
  2. Is the external clock reference sufficient to be the exclusive source for clock?

 

My hardware specs:

 

MK64FN1M0VLL12 (QFP100)

KSZ8081 (QFP32)

 

Thank you.

 

Marco

1 解答
1,488 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Marco,

 

Please refer to the reference manual in chapter 5.7.7

pastedImage_2.png

 

In this case the slowest clock source you can use is an external clock in OSCERCLK or ENET_1588_CLKIN that can give you up to 50 MHz. Otherwise you will have to use the internal source clock (Core/System clock, MCG PLL/FLL clock) that work at 120 MHz.

Is the external clock reference sufficient to be the exclusive source for clock?

Yes, just keep in mind that the clock period should be an integer number of nanoseconds.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,489 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Marco,

 

Please refer to the reference manual in chapter 5.7.7

pastedImage_2.png

 

In this case the slowest clock source you can use is an external clock in OSCERCLK or ENET_1588_CLKIN that can give you up to 50 MHz. Otherwise you will have to use the internal source clock (Core/System clock, MCG PLL/FLL clock) that work at 120 MHz.

Is the external clock reference sufficient to be the exclusive source for clock?

Yes, just keep in mind that the clock period should be an integer number of nanoseconds.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,488 次查看
marcoantoniodeo
Contributor II

Hi Felipe,

 

I´ve read that page but to be true your explanation makes more sense to me know.

 

Thank you

 

Marco