Hello everyone!
I am new to Freescale and Kinetis, so please forgive my RTFM-questions.
I have a K60 Tower development kit. I searched for a bootloader which should be able to load an application via Ethernet.
My first approach was to donload MQX 3.8.1 and try the bootloader example.
I noticed that there are configurations for various CPU's but not for the K60.
So I created an empty project for my CPU, copied the sources of the bootloader example into the sources directory and made my way through all the compiler errors until I had included the search paths for all the include files necessary. This went fine until a point where the compiler stopped at an error directive in adc.h like this:
This could mean that I included a wrong path somewhere or that the bootloader example should be modified to be used on the K60.
On the other hand, I found it surprising that I need an ADC for the bootloader.
I paused with this one and tried the "Ethernet Bootloader for the MCU" AN4367SW.zip.
The quick start guide tells me to use the mcp-file for my processor.
Well, there is a configuration directory mk60n512 which is not exactly my CPU but hopefully close enough.
The surprise is, that there is no mcp file in this directory. There are, however, mcp-files in the other konfiguration directories for other CPU's.
Here I go again....
My question is: Am I completely off the mark with my approaches, what would be a good approach?
Or should I go ahead and modify the examples if needed and hope to get a working Software in the end?
Greetings, Martin
已解决! 转到解答。
Hi martinpi, I invite you to check our Ethernet bootloader application note AN4367, it includes the fully functional code example, it was implemented and tested in the K60 platform:
Documentation:
http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf
You can find the code example as AN4367SW in our website
Hi martinpi, I invite you to check our Ethernet bootloader application note AN4367, it includes the fully functional code example, it was implemented and tested in the K60 platform:
Documentation:
http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4367.pdf
You can find the code example as AN4367SW in our website