Error with CW 10.2 and MQX3.8 TWRK60D100M?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error with CW 10.2 and MQX3.8 TWRK60D100M?

2,054 次查看
Bryan1z
Contributor I

I started a new build environment  using CW 10.2 and MQX TWRK60D10M.  After installing the MQX 3.8, I rebuild the library as suggested in the installation procedure. I ran into the following errors. How to work around this?

Description    Resource    Path    Location    Type

';' expected    main.c    /pe_demo_twrk60d100m/Source    line 299    C/C++ Problem

';' expected    main.c    /pe_demo_twrk60d100m/Source    line 300    C/C++ Problem

';' expected    main.c    /pe_demo_twrk60d100m/Source    line 301    C/C++ Problem

';' expected    main.c    /pe_demo_twrk60d100m/Source    line 431    C/C++ Problem

illegal implicit conversion from 'int' to 'int *'    main.c    /pe_demo_twrk60d100m/Source    line 233    C/C++ Problem

illegal implicit conversion from 'int' to 'int *'    main.c    /pe_demo_twrk60d100m/Source    line 310    C/C++ Problem

illegal implicit conversion from 'int' to 'int *'    main.c    /pe_demo_twrk60d100m/Source    line 391    C/C++ Problem

illegal implicit conversion from 'int' to 'int *'    main.c    /pe_demo_twrk60d100m/Source    line 440    C/C++ Problem

Link failed.    pe_demo_twrk60d100m             C/C++ Problem

Link failed.    secemail_twrk60d100m             C/C++ Problem

Link failed.    sectelnet_twrk60d100m             C/C++ Problem

Link failed.    secwebserver_twrk60d100m             C/C++ Problem

Link failed.    telnet2ser_twrk60d100m             C/C++ Problem

Link failed.    web_hvac_twrk60d100m             C/C++ Problem

mingw32-make: *** [intram_d.afx] Error 1    secemail_twrk60d100m             C/C++ Problem

mingw32-make: *** [intram_d.afx] Error 1    sectelnet_twrk60d100m             C/C++ Problem

mingw32-make: *** [intram_d.afx] Error 1    secwebserver_twrk60d100m             C/C++ Problem

mingw32-make: *** [intram_d.afx] Error 1    telnet2ser_twrk60d100m             C/C++ Problem

mingw32-make: *** [intram_d.afx] Error 1    web_hvac_twrk60d100m             C/C++ Problem

mingw32-make: *** [Source/main.obj] Error 1    pe_demo_twrk60d100m             C/C++ Problem

not an lvalue    main.c    /pe_demo_twrk60d100m/Source    line 571    C/C++ Problem

Overflow in segment: rom from section: .main_application Segment reserved size is: 0x0000fbe0 -- Overflow of: 0x00005c8c    telnet2ser_twrk60d100m             C/C++ Problem

Overflow in segment: rom from section: .main_application Segment reserved size is: 0x0000fbe0 -- Overflow of: 0x00008ab8    sectelnet_twrk60d100m             C/C++ Problem

Overflow in segment: rom from section: .main_application Segment reserved size is: 0x0000fbe0 -- Overflow of: 0x00009bf8    secemail_twrk60d100m             C/C++ Problem

Overflow in segment: rom from section: .main_application Segment reserved size is: 0x0000fbe0 -- Overflow of: 0x0000d6e0    secwebserver_twrk60d100m             C/C++ Problem

Overflow in segment: rom from section: .main_application Segment reserved size is: 0x0000fbe0 -- Overflow of: 0x0002fb54    web_hvac_twrk60d100m             C/C++ Problem

undefined identifier 'DA1_Device'    main.c    /pe_demo_twrk60d100m/Source    line 203    C/C++ Problem

undefined identifier 'DA1_Device'    main.c    /pe_demo_twrk60d100m/Source    line 204    C/C++ Problem

undefined identifier 'DA1_Error'    main.c    /pe_demo_twrk60d100m/Source    line 220    C/C++ Problem

undefined identifier 'DA1_Error'    main.c    /pe_demo_twrk60d100m/Source    line 223    C/C++ Problem

undefined identifier 'DA1_Error'    main.c    /pe_demo_twrk60d100m/Source    line 226    C/C++ Problem

undefined identifier 'DA1_Error'    main.c    /pe_demo_twrk60d100m/Source    line 515    C/C++ Problem

undefined identifier 'DA1_Error'    main.c    /pe_demo_twrk60d100m/Source    line 568    C/C++ Problem

undefined identifier 'DA1_Error'    main.c    /pe_demo_twrk60d100m/Source    line 611    C/C++ Problem

undefined identifier 'DA1_UserDataPtr'    main.c    /pe_demo_twrk60d100m/Source    line 202    C/C++ Problem

undefined identifier 'DA1_WatermarkValue'    main.c    /pe_demo_twrk60d100m/Source    line 570    C/C++ Problem

undefined identifier 'DA1_WatermarkValue'    main.c    /pe_demo_twrk60d100m/Source    line 574    C/C++ Problem

undefined identifier 'DA1_WatermarkValue'    main.c    /pe_demo_twrk60d100m/Source    line 613    C/C++ Problem

undefined identifier 'DA1_WatermarkValue'    main.c    /pe_demo_twrk60d100m/Source    line 614    C/C++ Problem

undefined identifier 'DA1_WatermarkValue'    main.c    /pe_demo_twrk60d100m/Source    line 616    C/C++ Problem

undefined identifier 'LDD_DAC_TBufferWatermark'    main.c    /pe_demo_twrk60d100m/Source    line 138    C/C++ Problem

undefined identifier 'LDD_TDeviceData'    main.c    /pe_demo_twrk60d100m/Source    line 135    C/C++ Problem

undefined identifier 'LDD_TError'    main.c    /pe_demo_twrk60d100m/Source    line 137    C/C++ Problem

undefined identifier 'LDD_TUserData'    main.c    /pe_demo_twrk60d100m/Source    line 136    C/C++ Problem

undefined identifier 'LED'    main.c    /pe_demo_twrk60d100m/Source    line 467    C/C++ Problem

undefined identifier 'LED'    main.c    /pe_demo_twrk60d100m/Source    line 470    C/C++ Problem

undefined identifier 'LED'    main.c    /pe_demo_twrk60d100m/Source    line 473    C/C++ Problem

undefined identifier 'LED'    main.c    /pe_demo_twrk60d100m/Source    line 481    C/C++ Problem

undefined identifier 'PWM_CNT_INP_FREQ_U_0'    main.c    /pe_demo_twrk60d100m/Source    line 323    C/C++ Problem

undefined identifier 'PWM_MaxValue'    main.c    /pe_demo_twrk60d100m/Source    line 321    C/C++ Problem

undefined identifier 'PWM_Step'    main.c    /pe_demo_twrk60d100m/Source    line 320    C/C++ Problem

undefined identifier 'PWM_Value'    main.c    /pe_demo_twrk60d100m/Source    line 319    C/C++ Problem

undefined identifier 'PWM_Value'    main.c    /pe_demo_twrk60d100m/Source    line 362    C/C++ Problem

undefined identifier 'PWM_Value'    main.c    /pe_demo_twrk60d100m/Source    line 365    C/C++ Problem

undefined identifier 'PWM_Value'    main.c    /pe_demo_twrk60d100m/Source    line 368    C/C++ Problem

undefined identifier 'TRG_CNT_INP_FREQ_U_0'    main.c    /pe_demo_twrk60d100m/Source    line 235    C/C++ Problem

undefined identifier 'TRG_CNT_INP_FREQ_U_0'    main.c    /pe_demo_twrk60d100m/Source    line 236    C/C++ Problem

undefined identifier 'WDog1_WATCHDOG_TIMEOUT'    main.c    /pe_demo_twrk60d100m/Source    line 401    C/C++ Problem

undefined identifier 'WDog1_WATCHDOG_WINDOW'    main.c    /pe_demo_twrk60d100m/Source    line 402    C/C++ Problem


标记 (3)
0 项奖励
回复
5 回复数

1,490 次查看
DavidS
NXP Employee
NXP Employee

Hi Bryan1z,

Two things to try:

1) Make sure CW10.2 has been updated (instructions below)

2) Open the FSL_MQX_in_CW_10_x.pdf (in C:\Freescale\Freescale MQX 3.8\doc\tools\cw) and do steps on slide 46 that re-generate the BSP to have PE code.

Hope this helps.

Regards,

David

Online update procedure:

A) If your computer is connected to the Internet, select

Install New Software in the Help Menu.

B) When the Installdialog is displayed, click the ‘Available SoftwareSites’ link.

C) When the Available Software Sitesdialog is displayed, click on the Freescale (link should be following:

     http://freescale.com/lgfiles/updates/Eclipse/MCU10_1/com.freescale.mcu.updatesite/

D) Before you can use the updated location, you must click on Test Connection.If you fail to

click on Test Connection, the location will be lostand you will need to restart at step C above

and fill in the entire url.

E) Now on the Available Software Sites Click OKand you are ready to update the software.

I check/enable all the options before doing updte.  Sometime I have to do update in two steps...MCU v10.2 Update 1.0.0 first then the MCU v10.2 Service Packs second.

1,490 次查看
Bryan1z
Contributor I

Hi David,

I updated all the patches, including the latest service pack for Windows from Freescale's website. I am one step closer to getting the sample code to run on the target.

I built and downloaded the hello application to the tower. It debugger complained that it can't open "MK60D10.mem" file, and bracket (twrk60d100m.mem).

0 项奖励
回复

1,490 次查看
DavidS
NXP Employee
NXP Employee

Hi Bryan1z,

Sorry for delay.

Are you running?

If not do you have MQX (and possible CW) installed to "C:\Program Files\Freescale\..." path on a Windows 7 machine?

If yes un-install and re-install CW and do updates.  Then install MQX.  But for both install to "C:\Freescale\...".

"Program Files" on Windows 7 has added protections that mess with CW and MQX.  So installing to another location resolves issues.

I just received my TWR-K60D100M, rebuilt the BSP and PSP, loaded hello example, selected the "Int Flash Debug" target and was able to program flash and execute the hello world.

I'm using the P&E Universal Multilink JTAG debugger hardware (it is fast than using the OSJTAG on board) so I updated my BSP twrk60d100m.h to use the TWR-SER serial interface.

#ifndef BSP_DEFAULT_IO_CHANNEL

    #if BSPCFG_ENABLE_TTYD

        #define BSP_DEFAULT_IO_CHANNEL                    "ttyd:"    /* TWR-SER     polled mode   */

        #define BSP_DEFAULT_IO_CHANNEL_DEFINED

    #else

        #define BSP_DEFAULT_IO_CHANNEL                      NULL

    #endif

#else

    /* undef is for backward compatibility with user_configh.h files which have already had it defined */

    #undef  BSP_DEFAULT_IO_CHANNEL_DEFINED

    #define BSP_DEFAULT_IO_CHANNEL_DEFINED

#endif

Regards,

David

0 项奖励
回复

1,490 次查看
Bryan1z
Contributor I

Hi David,

Thanks for the information. I re-install the system and it seems to behave now.

I am having trouble with displaying the printf on the eclipse console in MQX. I noticed you have commented on the IO Channel your e-mail, will this work with MQX? I checked online and forum, it seems that it doesn’t support it. Please advise.

I am using the TWRK60D100M for BSP development, my target doesn’t have serial interface. What is my option?

Thanks,

Bryan

0 项奖励
回复

1,490 次查看
DavidS
NXP Employee
NXP Employee

Hi Bryan1z,

C:\Freescale\Freescale MQX 3.8b1\doc\mqx\MQXIOUG.pdf

Read Chapter 22 Debug IO Driver.

In twrk60d100m.h

Use "iodebug:"   IDE debug...change header as follows:

    #if         #define BSPCFG_ENABLE_IODEBUG   "iodebug:"    /* IDE debug console...printf() written to console window of CW10.2*/

        #define BSP_DEFAULT_IO_CHANNEL_DEFINED

    #else

        #define BSP_DEFAULT_IO_CHANNEL                      NULL

    #endif

In your user_config.h

#define BSPCFG_ENABLE_IODEBUG    1     <-- Change from 0 to "1"

Lastly there is example:

C:\Freescale\Freescale MQX 3.8\mqx\examples\io_debug

Regards,

David

0 项奖励
回复