Enumerate OpenSDA serial number

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Enumerate OpenSDA serial number

1,516 次查看
samuelvestlin
Contributor II

I've noticed that when connecting more than one FRDM-KW41Z to my computer they all get the same OpenSDA/JLink serial number. This makes it impossible to differentiate between two boards when debugging or flashing using JLink. Is it possible to configure the OpenSDA serial number on the board and give it a unique number?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,332 次查看
BlackNight
NXP Employee
NXP Employee

On the real J-Links every J-Link has its own unique serial number.

I don't think it is possible to change that serial number, as it is the one programmed into the J-Link firmware binary.

At least on machine (Windows 10) I can differenciate them with the order they show up in the list/drop down, if they are always connected to the same USB port.

I hope this helps,

Erich

0 项奖励
回复

1,332 次查看
samuelvestlin
Contributor II

Yes, I've also noticed that the "real" J-Link has a unique serial number. Since OpenSDA is Open Source I was hoping to find a solution to generate new serial numbers. I was also hoping for it to be stored in the configuration memory area of the J-Link, i.e. visible when running J-Link command rconf. If so, it would be possible to set a new serial using wconf. But no luck finding it so far.

0 项奖励
回复