Eagle lbr

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Eagle lbr

3,517 次查看
manu_00
Contributor II

Hello,

does anybody know if there exists a eagle library for the Kinetis K_60 µC? And if yes, where can I find it.

Thanks,

Manu

标签 (1)
0 项奖励
回复
5 回复数

2,364 次查看
toñohernández
Contributor III

hello Manuel:

Sorry for the late response, I was looking for a response within our engineering team.

Currently we do not have available an Eagle Library for the K60 MCUs

We do have our Touch Sensing Software (TSS) and our Crypto Acceleration Unit (CAUAP) for both K60 100 and 120 MHz, and also MapuSoft's OS Changer Porting Kit for K60 100MHz... Chek them at:

K60_100 Product Summary Page

K60_120 Product Summary Page

What are you looking for? And maybe we can figure out a solution for your need.
Please let me know

2,364 次查看
manu_00
Contributor II

Hey,

thank you for the answer. I "built" the K60 by my own, so this issue is solved. :-)

Now i'm working on the next problem. I am using the K60DN256VQL10 and i am currious to know if it is possible to use Ethernet and Debugging at the same time? If yes how do i have to connect the debugg interface to the controller?

0 项奖励
回复

2,364 次查看
manu_00
Contributor II

I forgot to mention that i want to use SWV and ETM Interface.

0 项奖励
回复

2,364 次查看
apanecatl
Senior Contributor II

The answer is yes, you can use ethernet while debugging, regarding the necessary signals you need to connect the following lines from the debugger to the K60:

  1. JTAG_TMS / SWD_DIO
  2. JTAG_TCLK / SWD_CLK
  3. JTAG_TDI
  4. JTAG_TDO / TRACE_SWO
  5. JTAG_TRST_b  (optional)


2,364 次查看
manu_00
Contributor II

no answers at all?

0 项奖励
回复