EXT_SYNC signal connection via AOI-Module and crossbar: possible to miss??

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EXT_SYNC signal connection via AOI-Module and crossbar: possible to miss??

1,076 次查看
flowsn75
Contributor I

Hi,

I'm using a KV5x SoC for its DSP capabilities.

Mainly I'm using the PWM. 

I use the EXT_SYNC signal to generate a FORCE_OUT on PWM0 sub-modules 1 and 2. (sub-module 0 uses local sync), thus changing their outputs at the same, but variable instant (but with different dead-times)

The EXT_SYNC originating from an AND of a external comparator and from PWM1 peripheral output trigger.

Until know working fine.

However, in some cases I experience a problem: it very much seems that sub-module 2 receives that EXT_SYNC signal, generating FORCE_OUT, but sub-module 1 not!

So, my (generic) question is, is that even possible? Once the signal is put on the cross-bar by the AOI-Module, then going to the AHBP/AIPS, both requesting sub-modules of PWM0 should receive that EXT_SYNC signal, or not?? Or is there any chance of a phase-shift/delay in "sampling" that signal for each sub-module? As one can see, I'm not completely understanding how that signal gets from one peripheral to another.

 

In order to debug this issue, I output the signal coming from the AOI-module to a XB_OUT pin.

Comparing two cases, were in one case both sub-modules receive the EXT_SYNC and thus generate a FORCE_OUT event, and in the other case, were only sub-module 2 responds, the only difference I can see is that the signal at the XB_OUT pin in case of correct behavior is about (40ns pulse-length and 1.3V peak) and in case of failure is even more narrow (about 10ns and 0.8V peak).

 

As the configuration is very complex, I do not expect someone to go deep into it, I'd rather hope to get an answer to the above "generic" question.

 

Other info:

bus-clock 24MHz

core-clock 240MHz, PEE mode

Fast peripheral clock 120MHz

Nanoedge clock 240MHz

 

Thanks in advance to any clarifying Info.

 

 

 

0 项奖励
回复
3 回复数

1,017 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Thanks for contacting our technical support.

Are you considering that there is one EXT_SYNC signal for each submodule?

0 项奖励
回复

1,002 次查看
flowsn75
Contributor I

Hi Leo,

yes, of course, as I said, in 99% both sub-modules are receiving that signal and switch accordingly.

As described above, only if the signal coming from the AOI-Module has a very narrow pulse, I have the situation were only ONE sub-module switches, means executes the FORCE_OUT event.

Therefore my question, if the cross-bar passes the signal from the AOI-Module to one (connected) sub-module, it should in any case pass this also to the other connected sub-module, right? Or is there any chance, due to clocking or whatever, that one sub-module misses that very narrow signal?

0 项奖励
回复

848 次查看
_Leo_
NXP TechSupport
NXP TechSupport

Sorry for the delay. Could you send us (in a confidential ticket) your complete project to test the issue in the TWR-KV58F220M please?

0 项奖励
回复