Dose K60 support quad spi NOR flash mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dose K60 support quad spi NOR flash mode?

ソリューションへジャンプ
917件の閲覧回数
楊智翔楊
Contributor II

Dose the K60 support quad spi flash mode?If can't,is possible to use sdcard spi bsp driver to do it?How to do?Thanks!

NorFlash is Micron Serial NOR Flash Memory,model is N25Q064A.

0 件の賞賛
返信
1 解決策
769件の閲覧回数
cutworth
NXP Employee
NXP Employee

No, you cannot use K60 for connecting QuadSPI. QuadSPI requires four data lines while K60 SPI module can just support one data in and one data out like typical SPI interface. 

For connecting QuadSPI, you need to use K80.

Hao

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
770件の閲覧回数
cutworth
NXP Employee
NXP Employee

No, you cannot use K60 for connecting QuadSPI. QuadSPI requires four data lines while K60 SPI module can just support one data in and one data out like typical SPI interface. 

For connecting QuadSPI, you need to use K80.

Hao

0 件の賞賛
返信