Does the MKV31F512VLH12 have 5V tolerant I/O?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the MKV31F512VLH12 have 5V tolerant I/O?

452 Views
kylewagner
Contributor I

I'm looking at using the MKV31512VLH12 microcontroller and am curious if the component has 5V tolerant I/O. I can't seem to find anything on the datasheet.

Labels (1)
0 Kudos
1 Reply

342 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Kyle, I hope you're doing well!

 

The KV31F's Maximum Digital Input Voltage value is (Vdd + 0.3V), and the Maximum Digital Output Voltage is (Vdd - 0.5). The operating ranges for Vdd is from -0.3V to a Maximum of 3.8V.

 

For more information about the operating characteristics of the KV31F, you can check its datasheet, here.

 

Please let me know if you have any other questions.

 

Best regards,

Sebastian

0 Kudos